您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 短波通边缘迅速截止型滤光片 (126)

滤光片介绍

Optical Filters are used to selectively transmit or block certain wavelengths or wavelength ranges within optical systems.

立即查看 添加到收藏夹

Acktar 杂散光控制产品

Acktar Advanced Coatings produces light-absorbing components and materials to control stray light and eliminate noise from specular reflection.

立即查看 添加到收藏夹

滤光片镀膜-传统镀膜和硬质溅射镀膜的比较

Confused about the differences between traditional-coated and hard-coated optical filters?

立即查看 添加到收藏夹

偏振介绍-第二部分-波片和延迟片

Waveplates and retarders are optical components designed to transmit light while modifying its polarization state without attenuating, deviating, or displacing the beam.

立即查看 添加到收藏夹

通过光束合成增加功率

When measuring minuscule particles, many advanced Life Science applications require more power than one laser produces.

立即查看 添加到收藏夹

对比短波红外和可见光成像系统

SWIR, or short-wave infrared, is light invisible to the human eye but detectable by specialized infrared imaging lenses and cameras.

立即查看 添加到收藏夹

滤光片固定支架和可更换滤光片支架

Easily add and remove optical filters from any cage system setup after viewing this quick demonstration of integrating a filter holder plate and interchangeable filter holder using #86-018 and #85-649.

立即查看 添加到收藏夹

E 系列运动型光学反射镜调整架

E-Series Kinematic Optical Mounts provide high value and essential features for applications including lab use, prototyping, and system integration

立即查看 添加到收藏夹

偏振片介绍

Polarizers are used in a wide range of imaging and research and development applications.

立即查看 添加到收藏夹

光学镀膜新动态-增透膜对比滤光片镀膜

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he discusses anti-reflective (AR) coatings vs filter coatings

立即查看 添加到收藏夹

光学镀膜新动态-原型制作

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he discusses prototype qualifications including custom, stock and modified stock filter options.

立即查看 添加到收藏夹

窗口片介绍

Optical Windows provide protection between an optical system or sensitive electronics and an outside environment.

立即查看 添加到收藏夹

EO成像实验室3.5:背光

Learn how to specify imaging system components.

立即查看 添加到收藏夹

爱特蒙特光学制造:我们做到了

Edmund Optics (EO) manufactures over 5 million optical components every year at our global facilities in the Americas and Asia.

立即查看 添加到收藏夹

爱特蒙特光学的计量技术:测量是制造的关键环节

Learn about the metrology that Edmund Optics® uses to guarantee the quality of all optical components and assemblies.

立即查看 添加到收藏夹

爱特蒙特光学成像对比:为什么光学件那么重要

The success of your machine vision application depends on the quality of your optical components.

立即查看 添加到收藏夹

EO成像实验室3.2:W型照明结构

Learn how to specify imaging system components.

立即查看 添加到收藏夹

如何运用现货元件打造光隔离器

Many laser applications are prone to specular reflections back into the source, causing overheating and decreased stability and lifetime.

立即查看 添加到收藏夹

修改现货光学件:其他服务

Join Andrew Fisher, Manufacturing R&D Engineer at Edmund Optics, as he discusses some tips for modifying stock optical components to fit your application's needs.

立即查看 添加到收藏夹

EO 全球制造基地

Edmund Optics® (EO) manufactures millions of precision optical components and subassemblies every year in our 5 global manufacturing facilities.

立即查看 添加到收藏夹

光导介绍

Light pipes are optical components that are typically used to increase the uniformity of a light source or to direct light.

立即查看 添加到收藏夹

光学镀膜新动态-检验性能

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he discusses tips for verifying filter performance.

立即查看 添加到收藏夹

如何校准单片扩束镜

Monolithic Reflective Beam Expanders are ideal for applications requiring broadband or achromatic beam expansion.

立即查看 添加到收藏夹

偏振介绍-第一部分-偏振基础

Polarizers are optical components designed to filter, modify, or analyze the various polarization states of light.

立即查看 添加到收藏夹

远心照明

Telecentric illumination is quickly becoming the illumination of choice for precision metrology due to its ability to produce "hard" edges that can be easily analyzed.

立即查看 添加到收藏夹

复合抛物面聚光器介绍

Compound Parabolic Concentrators (CPCs) are concentrator lenses made from rotated parabolic shapes to create specific acceptance angles through which divergent light is collected.

立即查看 添加到收藏夹

选择合适的分光镜

Continuing from where Part I: X-Y Setup ends, learn how to add a Z-axis to an existing X-Y configuration to achieve three degrees of freedom.

立即查看 添加到收藏夹

如何准直激光系统

Join Chris Williams as he briefly explains the basics of how to align a laser system onto a target.

立即查看 添加到收藏夹

哪些重要概念可以帮助您选择光学安装座

Edmund Optics offers a variety of kinematic, bar-type, translating, ring, and modular mounting components.

立即查看 添加到收藏夹

如何利用光学透镜成像

Although a common misconception, individual optical lenses do not always form an image when the object plane is placed a focal length away from the lens.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号