您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 电动平台 (54)

选择手动调整台要注意哪些因素

Edmund Optics offers a variety of ball bearing, crossed roller bearing, dovetail, and rack and pinion translation stages for linear translation, rotary, and tip-tilt movement.

立即查看 添加到收藏夹

了解调整台的相关规格

To select the best translation stage, it is important to understand key specifications such as resolution, load capacity, travel, accuracy, repeatability, and wobble.

立即查看 添加到收藏夹

多轴调整台结构-第一部分:X-Y结构

Learn how to make repeatable adjustments in more than one direction for any demanding optics, imaging, or photonics application with this simple, three minute video.

立即查看 添加到收藏夹

偏振定向平面透镜产品介绍

Polarization Directed Flat Lenses, which are formed with polymerized liquid crystal thin-film, create a focal length that is dependent on polarization state.

立即查看 添加到收藏夹

多轴调整台结构-第二部分:X-Y-Z结构

Continuing from where Part I: X-Y Setup ends, learn how to add a Z-axis to an existing X-Y configuration to achieve three degrees of freedom.

立即查看 添加到收藏夹

E 系列运动型光学反射镜调整架

E-Series Kinematic Optical Mounts provide high value and essential features for applications including lab use, prototyping, and system integration

立即查看 添加到收藏夹

你会用光学件做什么_2014西部光电展

Watch EO employees as they take optics on adventures all around the world.

立即查看 添加到收藏夹

爱特蒙特光学能解决你的问题

Are you a victim of optical engineering fatigue?

立即查看 添加到收藏夹

技术EO:EyeTech Digital Systems的TM4仪器

The Future Depends on Optics®

立即查看 添加到收藏夹

液态镜头 M12 成像镜头

TECHSPEC® Liquid Lens M12 Imaging Lenses from Edmund Optics combine a high-resolution with the electronic auto-focus of an integrated liquid lens

立即查看 添加到收藏夹

哪些重要概念可以帮助您选择光学安装座

Edmund Optics offers a variety of kinematic, bar-type, translating, ring, and modular mounting components.

立即查看 添加到收藏夹

Optotune可调焦透镜介绍

Optotune Focus-Tunable lenses feature a liquid polymer substrate with continuous focusability.

立即查看 添加到收藏夹

液态 Cx 系列固定焦距镜头

TECHSPEC® Liquid Lens Cx Series Fixed Focal Length Lenses from Edmund Optics offer both high resolution and fast electronic focus.

立即查看 添加到收藏夹

组装液态 Cx 系列镜头

Learn how to insert a liquid lens into a modular TECHSPEC Liquid Lens Cx Series Fixed Focal Length Lens Assembly from Edmund Optics.

立即查看 添加到收藏夹

大尺寸万向节光学镜架

爱特蒙特光学(Edmund Optics)提供的大尺寸万向节光学镜架可用于将大尺寸精密光学元件(如反射镜)集成到 OEM 和台式系统中。

立即查看 添加到收藏夹

了解液态镜头技术

Liquid lenses can be used to maximize imaging system flexibility across a wide variety of applications requiring rapid focusing.

立即查看 添加到收藏夹

光学镀膜新动态-介绍

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he provides an overview to his webinar including: Key Terminology, Coating Technology, Cost Drivers, and Application Examples.

立即查看 添加到收藏夹

爱特蒙特光学的计量技术:测量是制造的关键环节

Learn about the metrology that Edmund Optics® uses to guarantee the quality of all optical components and assemblies.

立即查看 添加到收藏夹

光学镀膜新动态-镀膜技术

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he discusses coating technology including Ion Assisted Deposition (IAD) and Hard Sputtered.

立即查看 添加到收藏夹

光学镀膜新动态-关键指标

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he discusses critical system requirements to communicate

立即查看 添加到收藏夹

光学镀膜新动态-成本因素

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he discusses coating cost drivers and provides tips on ways to save.

立即查看 添加到收藏夹

光学镀膜新动态-原型制作

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he discusses prototype qualifications including custom, stock and modified stock filter options.

立即查看 添加到收藏夹

光学镀膜新动态-检验性能

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he discusses tips for verifying filter performance.

立即查看 添加到收藏夹

光学镀膜新动态-生命科学应用

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he discusses tips for verifying filter performance.

立即查看 添加到收藏夹

光学镀膜新动态-增透膜对比滤光片镀膜

Join Stephan Briggs, Biomedical Engineer at Edmund Optics, as he discusses anti-reflective (AR) coatings vs filter coatings

立即查看 添加到收藏夹

学习利用准直光确定光学透镜的焦距

Collimated light occurs when light rays travel parallel to each other.

立即查看 添加到收藏夹

Victor Tango AutoDrive:爱特蒙特光学案例研究

Edmund Optics is a sponsor of Victor Tango AutoDrive, a team of Virginia Tech students who competed to design and build a fully autonomous vehicle

立即查看 添加到收藏夹

锥透镜介绍

Axicons are conical-shaped optical components used to create a ring-shaped beam.

立即查看 添加到收藏夹

如何组建旋转接头

Quick demonstration with step-by-setup instructions for building an optical cage system swivel joint assembly.

立即查看 添加到收藏夹

EO成像实验室3.3:定向照明

Learn how to specify imaging system components.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号