您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 台式系统 (87)

如何准直激光系统

Join Chris Williams as he briefly explains the basics of how to align a laser system onto a target.

立即查看 添加到收藏夹

TECHSPEC光学笼式系统介绍

Designed for modularity and flexibility, Edmund Optics' TECHSPEC Optical Cage System components are high precision alternatives to complex optical alignment systems.

立即查看 添加到收藏夹

多轴调整台结构-第二部分:X-Y-Z结构

Continuing from where Part I: X-Y Setup ends, learn how to add a Z-axis to an existing X-Y configuration to achieve three degrees of freedom.

立即查看 添加到收藏夹

了解调整台的相关规格

To select the best translation stage, it is important to understand key specifications such as resolution, load capacity, travel, accuracy, repeatability, and wobble.

立即查看 添加到收藏夹

组装液态 Cx 系列镜头

Learn how to insert a liquid lens into a modular TECHSPEC Liquid Lens Cx Series Fixed Focal Length Lens Assembly from Edmund Optics.

立即查看 添加到收藏夹

选择手动调整台要注意哪些因素

Edmund Optics offers a variety of ball bearing, crossed roller bearing, dovetail, and rack and pinion translation stages for linear translation, rotary, and tip-tilt movement.

立即查看 添加到收藏夹

多轴调整台结构-第一部分:X-Y结构

Learn how to make repeatable adjustments in more than one direction for any demanding optics, imaging, or photonics application with this simple, three minute video.

立即查看 添加到收藏夹

液态 Cx 系列固定焦距镜头

TECHSPEC® Liquid Lens Cx Series Fixed Focal Length Lenses from Edmund Optics offer both high resolution and fast electronic focus.

立即查看 添加到收藏夹

对比短波红外和可见光成像系统

SWIR, or short-wave infrared, is light invisible to the human eye but detectable by specialized infrared imaging lenses and cameras.

立即查看 添加到收藏夹

E 系列运动型光学反射镜调整架

E-Series Kinematic Optical Mounts provide high value and essential features for applications including lab use, prototyping, and system integration

立即查看 添加到收藏夹

滤光片镀膜-传统镀膜和硬质溅射镀膜的比较

Confused about the differences between traditional-coated and hard-coated optical filters?

立即查看 添加到收藏夹

可更换的光学安装座和侧面接入安装板

This is a quick video demonstration of integrating an optical cage system interchangeable optical mount and side access mounting plate using #85-717 and #85-641.

立即查看 添加到收藏夹

可插入四根支杆的连接板

This is a quick demonstration of integrating a four-rod insertion plate with a sample cage system using #85-643.

立即查看 添加到收藏夹

如何组建旋转接头

Quick demonstration with step-by-setup instructions for building an optical cage system swivel joint assembly.

立即查看 添加到收藏夹

大尺寸万向节光学镜架

爱特蒙特光学(Edmund Optics)提供的大尺寸万向节光学镜架可用于将大尺寸精密光学元件(如反射镜)集成到 OEM 和台式系统中。

立即查看 添加到收藏夹

LC(低成本)定倍YAG扩束镜

LC (Low Cost) Fixed YAG Beam Expanders are simple 2-element, cost-effective solutions to beam expansion.

立即查看 添加到收藏夹

最优方法#2—别相信你的眼睛

Join Greg Hollows, Director of the Imaging Business Unit and EO's Imaging Expert, as he reviews some Best Practice to consider when designing an imaging system.

立即查看 添加到收藏夹

激光光学实验室: 扩束镜结构及设计

Laser beam expanders consist of transmissive configurations, with Galilean or Keplerian designs, and reflective configurations, which use a series of mirrors, similar to microscope designs.

立即查看 添加到收藏夹

滤光片固定支架和可更换滤光片支架

Easily add and remove optical filters from any cage system setup after viewing this quick demonstration of integrating a filter holder plate and interchangeable filter holder using #86-018 and #85-649.

立即查看 添加到收藏夹

2012节日特辑:僵尸大战

Happy Holidays from EO! Friends, is this not what the holidays are all about?

立即查看 添加到收藏夹

Danfoss:爱特蒙特光学案例研究

Monitoring and regulating air pollution is an essential step towards creating a cleaner environment.

立即查看 添加到收藏夹

EO成像实验室1.7:深入了解对比度

Learn how to specify imaging system components.

立即查看 添加到收藏夹

最优方法#9—学会控制

Join Greg Hollows, Director of the Imaging Business Unit and EO's Imaging Expert, as he reviews some best practices to consider when designing an imaging system.

立即查看 添加到收藏夹

EO成像实验室1.6:深入了解分辨率

Learn how to specify imaging system components.

立即查看 添加到收藏夹

液态镜头 M12 成像镜头

TECHSPEC® Liquid Lens M12 Imaging Lenses from Edmund Optics combine a high-resolution with the electronic auto-focus of an integrated liquid lens

立即查看 添加到收藏夹

EO成像实验室1.8:深入了解景深

Learn how to specify imaging system components.

立即查看 添加到收藏夹

最优方法#1—空间越大越好

Join Greg Hollows, Director of the Imaging Business Unit and EO's Imaging Expert, as he reviews some Best Practice to consider when designing an imaging system.

立即查看 添加到收藏夹

最优方法#3—别离的太近

Join Greg Hollows, Director of the Imaging Business Unit and EO's Imaging Expert, as he reviews some Best Practice to consider when designing an imaging system.

立即查看 添加到收藏夹

最优方法#5—颜色事宜

Join Nick Sischka, Vision Solutions Specialist and member of EO's Imaging Team, as he reviews some best practices to consider when designing an imaging system.

立即查看 添加到收藏夹

最优方法#11—做一个清单

Join Greg Hollows, Director of the Imaging Business Unit and EO’s Imaging Expert, as he reviews some best practices to consider when designing an imaging system.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号