Edmund Optics®, a renowned provider of optical components, continuously expands its product offering to reflect market developments and customer needs. New products are added each month to better serve the industry. EO has added an additional variety of new sizes and optical coatings for many off-the-shelf optical components, reducing the costs and lead times of rapid prototyping. This expanded product offering is available for immediate shipping, benefiting applications requiring small order quantities and quick prototyping, as it reduces the need for cost-prohibitive, low-volume custom solutions.
The TECHSPEC® Sapphire Windows are one of the product lines with an expanded offering of sizes and coating options. These windows, which are manufactured from a single crystal of aluminum oxide (Al2O3) sapphire, are now available with new infrared broadband anti-reflection (BBAR) coatings that expand the total covered wavelength range to 400 - 5000nm. These windows are ideal for harsh environment applications due to their extreme surface hardness, high thermal conductivity, high dielectric constant, and resistance to common chemical acids and alkalis.
The TECHSPEC® Ultrafast-Enhanced Silver Concave Laser Mirrors now include coating options for 800 - 1150nm wavelengths for Yb-doped lasers in addition to previous coatings tailored for Ti:sapphire lasers. With their extremely low group delay dispersion (GDD) as low as 0 ±20fs2, are ideal for low- to medium-power ultrafast applications requiring broad bandwidths.
To view these, and many more exciting new products offered by Edmund Optics, visit the new products page at www.edmundoptics.com.
About EO:
Edmund Optics® (EO) is a leading global supplier of optics, imaging, and photonics technology that has served a variety of markets including Life Sciences, Biomedical, Industrial Inspection, Semiconductor, R&D, and Defense since 1942. EO designs and manufactures a wide array of optical components, multi-element lenses, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of stock and custom products. With locations in more than nine countries across the globe, EO employs just over 1,000 employees and continues to expand. Customers can purchase items by calling 1-800-363-1992, via the catalog, or on the website at www.edmundoptics.com.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号