您选择的产品已被添加至购物车
All Press Releases

Eradicate Chromatic Aberrations and Dispersion with New Achromatic Singlet Lenses and Low GDD Ultrafast Mirrors

11/25/2020, Barrington, NJ USA   —

Edmund Optics®, a renowned provider of optical components, continuously expands its product offering to reflect market developments and customer needs. New products are added each month to better serve the industry. EO just released TECHSPEC® Achromatic Singlet Lenses, which are ideal for broadband focusing applications, and TECHSPEC® High Performance Low GDD Ultrafast Mirrors, which are used for minimizing dispersion in ultrafast systems. No matter how chromatic effects are hindering your system performance, EO has your solution.

TECHSPEC Achromatic Singlet Lenses correct for chromatic focal shift using a unique geometry rather than two separate materials. They are diamond turned aspheric achromatic lenses made of Zeonex E48R and are ideal for broadband focusing applications as well as ultraviolet applications where optical cement is undesired. These lenses outperform traditional achromatic doublets by a factor of 3 and plano-convex (PCX) singlets by a factor of nearly 40 in terms of chromatic focal shift.

The TECHSPEC High Performance Low GDD Ultrafast Mirrors are designed to have high reflectivity at a 45° angle of incidence, which is ideal for ultrafast laser beam steering applications like the transport of femtosecond laser pulses. These mirrors feature an ion beam sputtered (IBS) dispersion-compensating coating that provides lower scatter and absorption than traditional dielectric laser mirrors. The group delay dispersion (GDD) of the TECHSPEC High Performance Low GDD Ultrafast Mirrors is near zero at their design wavelength ranges, which minimizes dispersion of the reflected beam.

To view these, and many more exciting new products offered by Edmund Optics, visit the new products page at www.edmundoptics.com.

About EO:

Edmund Optics® (EO) is a leading global supplier of optics, imaging, and photonics technology that has served a variety of markets including Life Sciences, Biomedical, Industrial Inspection, Semiconductor, R&D, and Defense since 1942. EO designs and manufactures a wide array of optical components, multi-element lenses, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of stock and custom products. With locations in more than nine countries across the globe, EO employs just over 1,000 employees and continues to expand. Customers can purchase items by calling 1-800-363-1992, via the catalog, or on the website at www.edmundoptics.com.

 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号