您选择的产品已被添加至购物车
All Press Releases

Aspheres from Edmund Optics® Simplify Optical Designs and Improve Precision Performance

2/22/2022, Barrington, NJ USA   —

Edmund Optics®, a leading global manufacturer and supplier of optical components, has expanded its extensive inventory by bolstering its offering of aspheres ideal for a wide range of unique and demanding applications. This product expansion includes the TECHSPEC® Double-Sided Aspheric Lenses ideal for imaging applications and the TECHSPEC® Near-Infrared Precision Aspheric Lenses for enabling high precision performance. These aspheres are two products out of a much larger selection of new aspheres from Edmund Optics. This new selection provides optical integrators an increased number of options for the specific demands of their applications, enabling rapid prototyping and product development.

Aspheres are optical lens elements with at least one non-flat, non-spherical surface. There are a number of benefits associated with using an asphere over a spherical lens element such as the elimination of spherical aberration, superior focusing ability for smaller spot sizes and reduced blur, and better light collection. Aspheres are commonly used as a lighter and smaller alternative to using a series of spherical components to accomplish the same result in a lens assembly. Edmund Optics currently offers a wide range of different aspheres and possesses extensive asphere design, manufacturing, and metrology expertise. Manufacturing thousands of precision aspheres each month Edmund Optics holds a large inventory of standard and high precision lenses for immediate delivery and extends its offerings continuously, reflecting the needs of markets and customers.

The TECHSPEC® Double-Sided Aspheric Lenses feature high numerical apertures, diameter options from 10mm to 500mm, and are excellent options ideal for light collection or for 1:1 imaging applications. The double-convex or bi-convex design is used to reduce the number of optical elements in the optical system and consolidate the system space and weight for superior performance.

TECHSPEC® Near-Infrared (NIR) Precision Aspheric Lenses are optimized to eliminate spherical aberration in the near-infrared spectrum. These aspheric lenses are manufactured from S-LAH64 or N-BK7 substrates and polished through a computer numerical controlled (CNC) machining process to achieve high-precision performance. While the uncoated substrate option is designed for 780nm, other coatings options are available for 350-700nm, 600-1050nm, and 900-1700nm.

To view these, and many more exciting new products offered by Edmund Optics, visit the new products page at www.edmundoptics.com.

About Edmund Optics:

Edmund Optics® is a leading global supplier of optics, imaging, and photonics technology that has served a variety of markets including Life Sciences, Biomedical, Industrial Inspection, Semiconductor, R&D, and Defense since 1942. The company designs and manufactures a wide array of optical components, multi-element lenses, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of stock and custom products. Operating in more than a dozen major facilities around the globe, Edmund Optics employs just over 1,100 employees and continues to expand. Customers can purchase items by calling 1-800-363-1992, via the catalog, or on the website at www.edmundoptics.com.

 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号