您选择的产品已被添加至购物车

Why Should I Use a Lens Designed Specifically for SWIR Wavelengths?

Short wave infrared (SWIR) imaging optics are used for a vast array of applications including surveillance, semiconductor inspection, food and beverage inspection, and process quality control. These systems require specialized imaging optics, as lenses designed for visible use are not optimized for SWIR wavelengths and will suffer from chromatic aberrations and transmission losses. Edmund Optics® offers SWIR imaging lenses designed, coated, and tested at SWIR wavelengths, which are available at www.edmundoptics.com/3444

相关产品

本内容对您是否有用?

产品概述

}
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号