Beam Displacement, s (mm) : --
Displacement of Secondary Reflection, x (mm): --
$$ s = t \cdot \sin{\theta} \left( 1 - \frac{\cos{\theta}}{\sqrt{n^2 - \sin^2{\theta}}} \right) $$ |
$$ x = \frac{t \cdot \sin{\left( 2 \theta \right)}}{\sqrt{n^2 - \sin^2{\theta}}} $$ |
s | Beam Displacement |
x | Displacement of secondary reflection |
θ | Angle of incidence between beam and plate normal |
t | Thickness of plate |
n | Refractive index of medium |
Determine the displacement of a collimated beam incident on a tilted plane-parallel plate, or window. This displacement is dependent on the angle of incidence, the thickness of the plate, and the refractive index of the plate. This calculator also determines the displacement of the secondary reflection resulting from a small portion of the beam reflecting off the glass-air interface of the plate.
The exit beam will be parallel to the input beam and magnification remains constant when imaging through a plane-parallel plate.
Question: What is the displacement of a beam and its secondary reflection when the beam passes through a 10mm thick N-BK7 plate at an angle of incidence of 15 degrees?
Answer: The beam displacement and secondary reflection displacement can be determined by:
The displacement of the beam is 0.916mm and the displacement of the beam’s secondary reflection is 3.499mm.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号