您选择的产品已被添加至购物车

What happens when an optical filter is tilted?

Generally, as the angle of incidence increases a filter's transmission curve will shift to lower wavelengths. The effect of large angles from the center of the optical system is the same as tilting a filter from a perpendicular position to an optical system. As the angle of tilt gets larger, the curve will start to change shape, causing the transmission to steadily drop and the transmission curve slope to change. A similar effect is noticed as temperature increases. Interference filters are the most sensitive to angle of incidence and temperature.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号