您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 激光器 (127)

如何准直激光系统

Join Chris Williams as he briefly explains the basics of how to align a laser system onto a target.

立即查看 添加到收藏夹

如何运用现货元件打造光隔离器

Many laser applications are prone to specular reflections back into the source, causing overheating and decreased stability and lifetime.

立即查看 添加到收藏夹

复合抛物面聚光器介绍

Compound Parabolic Concentrators (CPCs) are concentrator lenses made from rotated parabolic shapes to create specific acceptance angles through which divergent light is collected.

立即查看 添加到收藏夹

激光光学实验室:激光器规格的选择

When determining which laser to use for your application, consider the following specifications: wavelength, coherence length, beam divergence, and Rayleigh range.

立即查看 添加到收藏夹

通过光束合成增加功率

When measuring minuscule particles, many advanced Life Science applications require more power than one laser produces.

立即查看 添加到收藏夹

单点金刚石车削:爱特蒙特光学(Edmund Optics)依图制造

Edmund Optics utilizes Diamond Turning to produce a wide range of high precision optical components.

立即查看 添加到收藏夹

激光光学实验室:预告

The Laser Optics Lab video series discusses laser optics concepts including specifications, coating technologies, product types, and more

立即查看 添加到收藏夹

激光光学实验室:简介

The Laser Optics Lab video series discusses laser optics concepts including specifications, coating technologies, product types, and more

立即查看 添加到收藏夹

光导介绍

Light pipes are optical components that are typically used to increase the uniformity of a light source or to direct light.

立即查看 添加到收藏夹

EO成像实验室1.5:传感器尺寸

Learn how to specify imaging system components.

立即查看 添加到收藏夹

Acktar 杂散光控制产品

Acktar Advanced Coatings produces light-absorbing components and materials to control stray light and eliminate noise from specular reflection.

立即查看 添加到收藏夹

爱特蒙特光学的计量技术:测量是制造的关键环节

Learn about the metrology that Edmund Optics® uses to guarantee the quality of all optical components and assemblies.

立即查看 添加到收藏夹

EO成像实验室3.5:背光

Learn how to specify imaging system components.

立即查看 添加到收藏夹

激光光学实验室: 激光镀膜

Optical coatings are composed of thin-film layers used to enhance transmission or reflection properties within an optical system.

立即查看 添加到收藏夹

大尺寸万向节光学镜架

爱特蒙特光学(Edmund Optics)提供的大尺寸万向节光学镜架可用于将大尺寸精密光学元件(如反射镜)集成到 OEM 和台式系统中。

立即查看 添加到收藏夹

爱特蒙特光学成像对比:为什么光学件那么重要

The success of your machine vision application depends on the quality of your optical components.

立即查看 添加到收藏夹

激光光学实验室:背向反射

Back reflections are created when some or part of your beam are reflected back to the source.

立即查看 添加到收藏夹

Danfoss:爱特蒙特光学案例研究

Monitoring and regulating air pollution is an essential step towards creating a cleaner environment.

立即查看 添加到收藏夹

分光镜介绍

Beamsplitters do exactly what their name implies: split incident light beams.

立即查看 添加到收藏夹

滤光片介绍

Optical Filters are used to selectively transmit or block certain wavelengths or wavelength ranges within optical systems.

立即查看 添加到收藏夹

学习利用准直光确定光学透镜的焦距

Collimated light occurs when light rays travel parallel to each other.

立即查看 添加到收藏夹

光学引领未来

Optics and the manipulation of light are critical for countless applications that save lives and improve quality of life across the world

立即查看 添加到收藏夹

光学件清洁指南

Knowing how to properly clean your optical components is an easy way to maintain system performance and save money by decreasing the risk of component damage.

立即查看 添加到收藏夹

选择合适的分光镜

Continuing from where Part I: X-Y Setup ends, learn how to add a Z-axis to an existing X-Y configuration to achieve three degrees of freedom.

立即查看 添加到收藏夹

2013光学行业独家解析

Edmund Optics' Chief Operating Officer, Samuel Sadoulet, provides his inside perspective on the optics industry for 2013.

立即查看 添加到收藏夹

如何正确处理光学件

Are you unsure of proper optics handling techniques?

立即查看 添加到收藏夹

如何利用光纤实现最佳准直

Collimated light is required for many fiber optic applications. Using the proper setup, fiber optic collimating lenses or ball lenses, and some optical know-how, you can achieve optimal collimation.

立即查看 添加到收藏夹

如何利用光学透镜成像

Although a common misconception, individual optical lenses do not always form an image when the object plane is placed a focal length away from the lens.

立即查看 添加到收藏夹

技术EO:EyeTech Digital Systems的TM4仪器

The Future Depends on Optics®

立即查看 添加到收藏夹

爱特蒙特光学70周年

Celebrate 70 years with EO! Take a journey from 1942 to 2012 and beyond.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号