您选择的产品已被添加至购物车
Open-Source DIY Microscopy

Bringing Professional-Grade Technology to All

 

Leveraging common mobile devices including smartphones and tablets

 

Previously cost-prohibitive technology more accessible

 

Consumer electronics integrated into research, industrial, and medical technologies

 

Including testing equipment, medical devices, thermal cameras, spectrometers, and more

Smartphones, tablets, wearable technology like smartwatches, and other modern consumer electronics provide unprecedented levels of portable computing power and connectivity. Research, industrial, and medical technologies are now integrating mobile devices into their designs, leveraging the prevalence of these powerful mobile devices to greatly reduce costs and make previously cost-prohibitive technology accessible to everyone. Technologies now integrated with consumer electronics include testing equipment, medical devices, thermal cameras, spectrometers, and more.

Integration into Laboratory Equipment

Universities and research institutions often require many different types of laboratory equipment including oscilloscopes, spectrum analyzers, and lock-in amplifiers. Acquiring all of these different devices can be costly and inaccessible for some labs. However, the integration of consumer electronics into laboratory equipment can drastically reduce the cost of equipment and even reduce the number of devices required.

Moku:Lab Multi-Instrument Device

The Moku:Lab Multi-Instrument Device eliminates the need for multiple laboratory testing and measurement devices by combining them into one compact device. Controlled via an intuitive iPad® interface, the Moku:Lab allows users to switch between instruments in real time. Additionally, settings such as scales, measurements, cursors, and input impedance are saved automatically when switching between instruments. The device features 2 high-speed channel analog (BNC) inputs and outputs and is compatible with Python, LabVIEW™, and MATLAB®. The Moku:Lab Multi-Instrument Device provides the means for professional-grade testing and measurement at new, lower levels of affordability and flexibility.

Tablet-Enabled All-in-One Multi-Instrument Device

Figure 1: Tablet-Enabled All-in-One Multi-Instrument Device

10 Instruments Included:
  • Oscilloscope
  • Lock-In Amplifier
  • Arbitrary Waveform Generator
  • Digital Filter Box
  • Phasemeter
  • Waveform Generator
  • PID Controller
  • Data Logger
  • Spectrum Analyzer
  • Bode Analyzer
Oscilloscope

Figure 2: Oscilloscope

Lock-In Amplifier

Figure 3: Lock-In Amplifier

Phasemeter

Figure 4: Phasemeter

Data Logger

Figure 5: Data Logger

Integration into Medical Devices

Integration into Medical Devices

Healthcare is heavily reliant on utilizing the best, most up-to-date equipment available to provide the highest quality medical services. Medical devices can greatly reduce production costs by leveraging the cameras, recording capabilities, and processing power of mobile devices. Some examples include the Oto Pro, a smartphone-enabled otoscope used to diagnose chronic ear infections in children, and OEM medical machines like oxygenators and wearable dialysis machines that use tablets as control units.

Biotechnology

Integration with Industrial Equipment

A wide range of industrial technologies are also integrating consumer electronics to significantly reduce costs and simplify use. FLIR Systems, Inc. offers a thermal imaging camera attachment for smartphones called FLIR ONE® that can be used to identify electrical problems, HVAC issues, and water leaks in roofs. A wide number of smartphone-enabled spectrometers have also been developed to identify unknown materials by breaking down the light that it reflects or emits.

FAQ's

FAQ  Is it possible to control the Moku:Lab Multi-Instrument Device without an iPad®?

Yes, there is an available Python library available from Liquid Instruments that allows you to interact with the Moku:Lab device from any computer running macOS, Windows, or Linux.

FAQ  Does Edmund Optics® sell the FLIR ONE® from FLIR Systems, Inc?
No, Edmund Optics® does not sell the FLIR ONE® from FLIR Systems, Inc.
FAQ  What would I use a smartphone enabled thermal camera for?
A smartphone-enabled thermal camera can use infrared imaging in a wide variety of applications including identifying where doors and windows are not well insulated, locating electrical problems by pinpointing heat build-up, and identifying issues in HVAC and plumbing systems. There are many applications and the list will continue to grow dramatically as customers discover this unseen portion of the electromagnetic spectrum.
 

Contact Us 

What limitations do you face today in your optics applications? What are the next problems that you need to be solved? Contact us today to work with our team of engineers to discover solutions to your application questions.

 
本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号