您选择的产品已被添加至购物车

Telecentric Lens

A type of imaging lens in which the exit pupil is located at infinity. As a result, within a certain range of working distances there is no viewing angle error or magnification error associated with features in the image that are at different heights or angles.

See also Magnification

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号