您选择的产品已被添加至购物车

Spatial Filter

An assembly that is used in conjunction with laser applications to eliminate spatial noise. A pinhole is used to select only the central peak of the intensity pattern from a focused spot. The size of the pinhole is selected based upon the wavelength, objective focal length, and input beam diameter.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号