A type of diffraction grating with a sawtooth profile that is generated by precision mechanical ruling engines. Replicas are then generated by depositing a coating, an epoxy layer, and polished substrate onto the master. Although the gratings are generally cut from larger pieces and have grooves across the entire face, incident light should be confined to 90% of the full face during use.
See also Diffraction Grating , Holographic Grating , Blaze Angle , Grating Equation , Groove Density , Relative Efficiency
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号