您选择的产品已被添加至购物车

Modulation Transfer Function (MTF)

A measure of contrast as a function of spatial frequency. Defined as 100% at zero-frequency, MTF continuously declines with increasing spatial frequency to zero contrast at a theoretical maximum resolution frequency defined by the diffraction limit of the optical system.

See also Diffraction Limit , Contrast , Resolution

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号