您选择的产品已被添加至购物车

Laser

Acronym that stands for light amplification by stimulated emission of radiation.  The basic structure is based on an active medium (either a gas or semiconductor) contained between two reflectors. A laser's reflectors contain light by oscillating it through a medium repeatedly allowing the energy to build up with each pass. Laser radiation escapes due to a partially reflecting mirror in the assembly.

See also Coherent Light , Gas Laser , Solid State Laser , Power Density , Spatial Mode , Warm-Up Time , Laser Damage Threshold , Modulation Bandwidth , Longitudinal Mode Spacing , Static Alignment

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号