您选择的产品已被添加至购物车

Infinite/Infinite Conjugate

A conjugate distance relationship that takes collimated light, changes the beam diameter according to the magnification, and emits collimated light. In terms of imaging, the object is placed at infinity (defined as the distance at which light rays can be considered collimated) in relation to the optical elements and relayed an infinite distance. No image is formed, but can be with the introduction of a secondary infinite/ finite conjugate design system.

See also Conjugate Distance , Double-Concave (DCV) Lens , Plano-Concave (PCV) Lens

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号