The ratio of the speed of light in a vacuum (c) to the speed of light in a refractive material (v). The index of refraction of a given medium varies with wavelength because the speed of light varies with wavelength. Common indices of refraction include nd (the yellow helium line at 587.6nm), nf (the blue hydrogen line at 486.1nm) and nc (the red hydrogen line at 656.3nm).
See also Abbe-Number , Birefringence , Angle of Incidence , Glass Code , Angle of Reflection , Dispersion , Refraction , Gradient Index , Cladding
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号