A type of manufacturing technique that starts with a standard spherical surface, such as an achromatic lens, which is pressed onto a thin layer of photopolymer in an aspheric mold to create an aspheric surface. After the surfaces are compressed and UV cured at room temperature, the end result is an aspherized achromatic lens that has chromatic and spherical aberration correction properties.
See also Aspheric Lens , Achromatic Lens
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号