您选择的产品已被添加至购物车

Beam Diameter

The calculated distance between two exactly opposed points on a beam at a chosen fraction of peak power (typically 1/e2). It is also defined as the diameter of a circular aperture that will pass a specified percentage (usually 90%) of the total beam energy.

See also Beam Divergence , Beam Expander , Beam Width

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号