您选择的产品已被添加至购物车

Ball Bearing Slide

A type of positioning component comprised of a stationary base with a mobile carriage riding on top. Two rows of hardened steel balls on both sides of the base provide the smooth, accurate, low friction sliding motion between the stationary base and the top slide.

See also Ball Bearing Stage , Thrust Capacity , Repeatability

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号