您选择的产品已被添加至购物车

Abbe-Number

Also known as Abbe constant, it inversely quantifies the amount of dispersion in an optical medium. It is given by a function of the refractive index of a material at the f (486.1nm), d (587.6nm), and c (656.3nm) wavelengths. A material with a high Abbe number means that the different wavelengths will have nearly the same index of refraction in that medium, yielding less separation between wavelengths of light.

See also Angle of Incidence , Glass Code , Angle of Reflection , Index of Refraction (n) , Dispersion

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号