您选择的产品已被添加至购物车

How do I mount a mirror to a mirror mount that doesn't have a clamp or retainer ring?

Mirrors are typically bonded to the aluminum mounting surface of a mirror mount with a two part adhesive. We carry Milbond Adhesive System, two part epoxy, which can be used for most glass-to-metal mirror bonding applications. This epoxy should be used for substrates that will not be subjected to very hostile environments.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号