您选择的产品已被添加至购物车

Does the circular polarizer material have to face a particular direction?

The linear polarizing side of the circular polarizer must face the observer. In this alignment, randomly polarized ambient light will be linearly polarized before it passes through the retarder side of the film and becomes circularly polarized. A quick test for orientation is to place a mirror behind the circular polarizer with a light source on the opposite viewing side. Upon reflection, the circularly polarized light is blocked from reaching the observer (in the form of glare). When the orientation is correct, the light reflecting from the mirror should not be visible. Randomly polarized light from the non-viewing side of the polarizer is allowed to pass through the material.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号