您选择的产品已被添加至购物车

Can wedge prisms be used for beam stearing?

Yes, a pair of wedge prisms can steer a beam anywhere within a circle described by the full angle 4θ, where θ is the deviation from a single prism. This beam steering is accomplished by rotating the two wedge prisms independently of each other, and is typically used to scan a beam to different locations in imaging applications. Two wedge prisms can be used as an anamorphic pair for beam shaping (to correct the elliptical shape of diode outputs).

Beam Steering with Wedge Prisms
本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号