Yes, ND (neutral density) filters exhibit an additive relationship with their optical density values. For instance, stacking filters with Optical Density values of 0.6 and 0.9 yield a resultant optical density of 1.5 (which gives an overall transmission of 3%) Care should be taken when using the reflective type of ND filter in order to insure that the reflected light does not interfere with the application. In stacks, the reflective filters are not parallel in order to reduce back reflections.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号