您选择的产品已被添加至购物车

What is the difference between refractive and diffractive line generators?

A refractive line generator uses a cylinder or rod lens to focus a laser in only one axis only (drop-moved placement) in order to create a line of light. A diffractive line generator uses a flat optic with an etched microstructure that breaks apart a laser beam and forms an interference pattern in the shape of a laser line. Refractive optics do not correct for the inherent Gaussian profile of a laser beam and form a line with a "hot spot" in the center and fading edges. Diffractive optics will create a line that is uniform in thickness over its length, but is segmented. Diffractive line generators also cause a small portion of the light to be redirected into different diffractive orders, which causes additional faint lines to appear. Some laser line generators use a unique patented Powell glass lens design in order to achieve a continuous (not segmented) line with an even distribution along the length of the line.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号