您选择的产品已被添加至购物车

Can I use an infinity-corrected objective in my microscope to get a longer working distance?

Only if your microscope is designed to work with an infinity-corrected objective. Due to the design of the infinity-corrected objective (see above question), they will not work in a DIN or JIS standard microscope. An infinity-corrected objective on a DIN or JIS standard microscope will not focus. Please also note that the threading for our infinity-corrected objectives is not a DIN standard threading and the objectives are physically not interchangeable with DIN or JIS objectives.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号