The most common adhesive we use for bonding our prisms is Norland NOA61. It is low-shrink (so the pieces won't move as it cures) and has excellent bonding strength for glass-to-glass. The adhesive is UV cured, so you'll need a UV source to make it stick. Once cured the adhesive is opaque to UV light but still works great if you are going to use the glued prism pair for visible or NIR applications, in other words, you can expect high transmission from 400 - 2000nm.
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号