Fiber optic light guides such as our Flexible Fiber Optic Light Guides consist of a bundle of high transmission glass fibers that can be used in conjunction with fiber optic illuminators to provide intense visible illumination. Fiber optic light guides and their respective illuminators are typically used for most fiber optic illumination applications. Quartz (or fused silica) fiber optic light guides such as our Quartz Fiber Optic Light Guides are designed for ultraviolet and infrared applications. They are ideal for UV transmission, but will transmit in the visible as well. They will also show some fluorescence at 245nm and darken in gamma or x-ray environments. These plastic-clad quartz fibers provide maximum transmission efficiency due to the 10:1 core/clad ratio and high flexibility from their small fiber diameter. Liquid fiber optic light guides such as our Liquid Light Guides are also ideal for visible and ultraviolet light applications. Unlike glass fiber optic bundles, liquid light guides are actually composed of liquid and do not suffer from packing fraction losses (spaces between fibers that cause reduced coupling efficiency).
或查看各区域电话
报价工具
只需输入商品编号
Copyright 2023, 爱特蒙特光学(深圳)有限公司。— 广东省深圳市龙华工业东路利金城科技工业园3栋5楼 518109 - 粤ICP备2021068591号