您选择的产品已被添加至购物车

What are the advantages of Fiber Optic Illumination?

Fiber optic light guides transmit light based on the principle of total internal reflection. Light incident on cylindrical fibers of either acrylic or glass materials can be transmitted through these fibers with little attenuation.

Useful for applications with very tight space or limited access constraints, Fiber Optic Illumination can provide a wide range of useful illumination geometries from spot lights and ring lights to diffuse sources and line lights. Light guide optics are also able to brave certain environments where using electronics would otherwise be a danger. Fiber optic illumination can also be intensity controlled and very easily aimed towards objects. Broadband illuminator sources provide white light illumination, which is composed of all of the colors of the visible spectrum.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号