您选择的产品已被添加至购物车

How do fiber optic light guides connect to fiber optic illuminators?

An adapter is required to connect our Fiber Optic Light Guides to our Fiber Optic Illuminators which all have a standard 25mm diameter opening port. Our Light Guide Adapters are metallic bushings with a ring shape designed to fit in the open aperture of our various illuminators. The light guide is inserted into the center hole of the adapter. The adapter and light guide are then held within the illuminator's aperture by a set screw. To select the correct adapter, you must match up the inner diameter of the adapter and the end-tip diameter of the light guide.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号