您选择的产品已被添加至购物车

I have two Basler Scout GigE cameras but I cannot use them simultaneously. When connected to a computer, either via two network cards or a single network card and a switch, they can be opened but cannot acquire images. What is causing the problem?

There are probably two issues at play that are cause the problem. First, make sure there is enough bandwidth for the amount of data to transfer. If this is insufficient, then the cameras won’t be able to acquire and transfer their data over the network. Second, it is known that GigE Cameras do not work the same with all network cards; it is best to use the recommended one though the manual does not require it.

本内容对您是否有用?
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号