Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 特种激光透镜 (134)

如何利用光学透镜成像

Although a common misconception, individual optical lenses do not always form an image when the object plane is placed a focal length away from the lens.

立即查看 添加到收藏夹

锥透镜介绍

Axicons are conical-shaped optical components used to create a ring-shaped beam.

立即查看 添加到收藏夹

学习利用准直光确定光学透镜的焦距

Collimated light occurs when light rays travel parallel to each other.

立即查看 添加到收藏夹

如何制造非球面透镜

Edmund Optics® manufactures thousands of precision aspheric lenses per month in our asphere manufacturing cell that operates 24 hours a day.

立即查看 添加到收藏夹

非球面消色差透镜介绍

Aspherized Achromatic Lenses, exclusive to Edmund Optics, are doublet lenses consisting of two cemented optical elements that are matched for their color-correction ability and small RMS spot size.

立即查看 添加到收藏夹

爱特蒙特光学的计量技术:测量是制造的关键环节

Learn about the metrology that Edmund Optics® uses to guarantee the quality of all optical components and assemblies.

立即查看 添加到收藏夹

如何准直激光系统

Join Chris Williams as he briefly explains the basics of how to align a laser system onto a target.

立即查看 添加到收藏夹

如何定义光学透镜的放大倍数

When doing basic imaging, how do you determine the magnification an optical lens will provide?

立即查看 添加到收藏夹

单点金刚石车削:爱特蒙特光学(Edmund Optics)依图制造

Edmund Optics utilizes Diamond Turning to produce a wide range of high precision optical components.

立即查看 添加到收藏夹

菲涅尔透镜介绍

Fresnel lenses are composed of a series of concentric grooves etched into one side of a sheet of plastic. Fresnel lenses are unlike typical spherical or aspherical optical lenses.

立即查看 添加到收藏夹

选择合适的分光镜

Continuing from where Part I: X-Y Setup ends, learn how to add a Z-axis to an existing X-Y configuration to achieve three degrees of freedom.

立即查看 添加到收藏夹

爱特蒙特光学制造:我们做到了

Edmund Optics (EO) manufactures over 5 million optical components every year at our global facilities in the Americas and Asia.

立即查看 添加到收藏夹

消色差透镜介绍

Learn about EO's most popular family of optical lenses and discover if achromatic lenses are ideal for your next application.

立即查看 添加到收藏夹

用于色散补偿的高色散超快反射镜

Learn how Highly-Dispersive Mirrors compensate for dispersion and compress pulse duration in ultrafast laser systems, which is critical for maximizing performance.

立即查看 添加到收藏夹

分光镜介绍

Beamsplitters do exactly what their name implies: split incident light beams.

立即查看 添加到收藏夹

Optotune可调焦透镜介绍

Optotune Focus-Tunable lenses feature a liquid polymer substrate with continuous focusability.

立即查看 添加到收藏夹

非球面透镜介绍

What is an aspheric lens? In what applications are aspheric lenses used?

立即查看 添加到收藏夹

偏振定向平面透镜产品介绍

Polarization Directed Flat Lenses, which are formed with polymerized liquid crystal thin-film, create a focal length that is dependent on polarization state.

立即查看 添加到收藏夹

Danfoss:爱特蒙特光学案例研究

Monitoring and regulating air pollution is an essential step towards creating a cleaner environment.

立即查看 添加到收藏夹

爱特蒙特光学成像对比:为什么光学件那么重要

The success of your machine vision application depends on the quality of your optical components.

立即查看 添加到收藏夹

如何运用现货元件打造光隔离器

Many laser applications are prone to specular reflections back into the source, causing overheating and decreased stability and lifetime.

立即查看 添加到收藏夹

爱特蒙特光学70周年

Celebrate 70 years with EO! Take a journey from 1942 to 2012 and beyond.

立即查看 添加到收藏夹

2014年 爱特蒙特光学公司的节日视频

As a family owned business for almost 75 years, the bond between family has long been the foundation of Edmund Optics.

立即查看 添加到收藏夹

Victor Tango AutoDrive:爱特蒙特光学案例研究

Edmund Optics is a sponsor of Victor Tango AutoDrive, a team of Virginia Tech students who competed to design and build a fully autonomous vehicle

立即查看 添加到收藏夹

选择合适的扩束镜

Edmund Optics offers both fixed power and zoom beam expanders. Knowing which beam expander is right for your application can greatly improve system efficiency.

立即查看 添加到收藏夹

复合抛物面聚光器介绍

Compound Parabolic Concentrators (CPCs) are concentrator lenses made from rotated parabolic shapes to create specific acceptance angles through which divergent light is collected.

立即查看 添加到收藏夹

Acktar 杂散光控制产品

Acktar Advanced Coatings produces light-absorbing components and materials to control stray light and eliminate noise from specular reflection.

立即查看 添加到收藏夹

加固成像镜头

Edmund Optics® manufactures several different types of ruggedized imaging lens assemblies.

立即查看 添加到收藏夹

LC(低成本)定倍YAG扩束镜

LC (Low Cost) Fixed YAG Beam Expanders are simple 2-element, cost-effective solutions to beam expansion.

立即查看 添加到收藏夹

如何校准单片扩束镜

Monolithic Reflective Beam Expanders are ideal for applications requiring broadband or achromatic beam expansion.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号