Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 激光扩束镜 (295)

激光扩束镜

Laser beam expanders are critical for reducing power density, minimizing beam diameter at a distance, and minimizing focused laser spot size.

立即查看 添加到收藏夹

LC(低成本)定倍YAG扩束镜

LC (Low Cost) Fixed YAG Beam Expanders are simple 2-element, cost-effective solutions to beam expansion.

立即查看 添加到收藏夹

扩束镜测试

Shack-Hartmann wavefront sensors are used to test the transmitted wavefront error of laser beam expanders, predicting the real-world performance of the beam expander.

立即查看 添加到收藏夹

如何校准单片扩束镜

Monolithic Reflective Beam Expanders are ideal for applications requiring broadband or achromatic beam expansion.

立即查看 添加到收藏夹

选择合适的扩束镜

Edmund Optics offers both fixed power and zoom beam expanders. Knowing which beam expander is right for your application can greatly improve system efficiency.

立即查看 添加到收藏夹

扩束镜选择指南

Not sure which beam expander will work best in your application? Check out EO's Beam Expander Selection Guide to easily compare each type at Edmund Optics.

立即查看 添加到收藏夹

如何利用现货光学件设计扩束镜

Are standard beam expanders not meeting your application requirements? Learn how to design your own beam expander using stock optics at Edmund Optics.

立即查看 添加到收藏夹

旋转与滑动扩束镜对焦机制

Sliding focusing mechanisms for laser beam expanders cause less beam wander than rotating focusing mechanisms, but they use more complex mechanics and are typically more expensive.

立即查看 添加到收藏夹

反射式光学元件适用于激光应用

Beam Conditioning Optics for UV, IR, and Broadband Lasers

立即查看 添加到收藏夹

2μm 激光器

The unique absorption properties of 2µm lasers allow them to create small and precise cuts for medical and materials processing applications

立即查看 添加到收藏夹

光束直径对激光损伤阈值的重要性

The diameter of a laser highly affects an optic’s laser induced damage (LIDT) as beam diameter directly impacts the probability of laser damage.

立即查看 添加到收藏夹

适用于激光应用的高反射率反射镜

The industry standard method for quantifying reflectivity does not tell the whole story

立即查看 添加到收藏夹

激光光学实验室: 扩束镜结构及设计

Laser beam expanders consist of transmissive configurations, with Galilean or Keplerian designs, and reflective configurations, which use a series of mirrors, similar to microscope designs.

立即查看 添加到收藏夹

高斯光束传播

Understanding Gaussian beam propagation is critical for understanding laser systems because many lasers are assumed to have Gaussian profiles.

立即查看 添加到收藏夹

激光系统的关键参数

了解确保激光应用成功必须考虑的关键参数。将为这些参数建立通用术语。

立即查看 添加到收藏夹

激光器谐振模

The length of a laser resonator determines the laser’s resonator modes, or the electric field distributions that cause a standing wave in the cavity.

立即查看 添加到收藏夹

高斯光束计算器

立即查看 添加到收藏夹

激光光学计量

Metrology is critical for ensuring that optical components consistently meet their desired specifications, especially in laser applications.

立即查看 添加到收藏夹

通过光束合成增加功率

When measuring minuscule particles, many advanced Life Science applications require more power than one laser produces.

立即查看 添加到收藏夹

光束质量和斯特列尔比

There are several metrics used to describe the quality of a laser beam including the M2 factor, the beam parameter product, and power in the bucket

立即查看 添加到收藏夹

高激光损伤AR镀膜

Laser optics high reflectivity mirrors meet exceptional specifications that Edmund Optics' competitors often fail to meet. Learn more at Edmund Optics.

立即查看 添加到收藏夹

分光镜介绍

Beamsplitters do exactly what their name implies: split incident light beams.

立即查看 添加到收藏夹

4 大光学前沿

Advances in microscopy, imaging, and extreme ultraviolet optics

立即查看 添加到收藏夹

如何准直激光系统

Join Chris Williams as he briefly explains the basics of how to align a laser system onto a target.

立即查看 添加到收藏夹

光学棱镜简介

Learn about the different types of optical prisms, their applications, and how to select the right prism for your specific system.

立即查看 添加到收藏夹

了解并指定激光元件的激光损伤阈值(LIDT)

Laser induced damage threshold (LIDT) denotes the maximum laser fluence an optical component can withstand with an acceptable amount of risk.

立即查看 添加到收藏夹

激光损伤阈值测试

Testing laser induced damage threshold (LIDT) is not standardized, so understanding how your optics were tested is critical for predicting performance.

立即查看 添加到收藏夹

超快激光的激光损伤阈值

The short pulse durations of ultrafast lasers make them interact with optical components differently, impacting the optic’s laser damage threshold.

立即查看 添加到收藏夹

带有激光照明的荧光成像

Fluorescence imaging systems are composed of three major components, an illumination source, a photo-activated fluorophore sample, and detector.

立即查看 添加到收藏夹

深入了解锥透镜

Axicons can be used in a variety of different fields. Find out more about axicons and how to use them in applications at Edmund Optics.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号