Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 激光偏振 (285)

激光器谐振模

The length of a laser resonator determines the laser’s resonator modes, or the electric field distributions that cause a standing wave in the cavity.

立即查看 添加到收藏夹

偏振片介绍

Polarizers are used in a wide range of imaging and research and development applications.

立即查看 添加到收藏夹

偏振介绍-第一部分-偏振基础

Polarizers are optical components designed to filter, modify, or analyze the various polarization states of light.

立即查看 添加到收藏夹

偏振介绍-第二部分-波片和延迟片

Waveplates and retarders are optical components designed to transmit light while modifying its polarization state without attenuating, deviating, or displacing the beam.

立即查看 添加到收藏夹

偏振定向平面透镜产品介绍

Polarization Directed Flat Lenses, which are formed with polymerized liquid crystal thin-film, create a focal length that is dependent on polarization state.

立即查看 添加到收藏夹

2μm 激光器

The unique absorption properties of 2µm lasers allow them to create small and precise cuts for medical and materials processing applications

立即查看 添加到收藏夹

激光光学计量

Metrology is critical for ensuring that optical components consistently meet their desired specifications, especially in laser applications.

立即查看 添加到收藏夹

激光系统的关键参数

了解确保激光应用成功必须考虑的关键参数。将为这些参数建立通用术语。

立即查看 添加到收藏夹

激光扩束镜

Laser beam expanders are critical for reducing power density, minimizing beam diameter at a distance, and minimizing focused laser spot size.

立即查看 添加到收藏夹

高激光损伤AR镀膜

Laser optics high reflectivity mirrors meet exceptional specifications that Edmund Optics' competitors often fail to meet. Learn more at Edmund Optics.

立即查看 添加到收藏夹

适用于激光应用的高反射率反射镜

The industry standard method for quantifying reflectivity does not tell the whole story

立即查看 添加到收藏夹

了解并指定激光元件的激光损伤阈值(LIDT)

Laser induced damage threshold (LIDT) denotes the maximum laser fluence an optical component can withstand with an acceptable amount of risk.

立即查看 添加到收藏夹

超快激光的激光损伤阈值

The short pulse durations of ultrafast lasers make them interact with optical components differently, impacting the optic’s laser damage threshold.

立即查看 添加到收藏夹

如何准直激光系统

Join Chris Williams as he briefly explains the basics of how to align a laser system onto a target.

立即查看 添加到收藏夹

如何运用现货元件打造光隔离器

Many laser applications are prone to specular reflections back into the source, causing overheating and decreased stability and lifetime.

立即查看 添加到收藏夹

常用激光光学材料

Understanding the most commonly used laser optics materials will allow for easy navigation of EO’s wide selection of laser optics components.

立即查看 添加到收藏夹

反射式光学元件适用于激光应用

Beam Conditioning Optics for UV, IR, and Broadband Lasers

立即查看 添加到收藏夹

激光损伤阈值测试

Testing laser induced damage threshold (LIDT) is not standardized, so understanding how your optics were tested is critical for predicting performance.

立即查看 添加到收藏夹

Coherent® 激光器选择指南

Compare Coherent Laser specifications with the Edmund Optics selection guide.

立即查看 添加到收藏夹

带有激光照明的荧光成像

Fluorescence imaging systems are composed of three major components, an illumination source, a photo-activated fluorophore sample, and detector.

立即查看 添加到收藏夹

超快激光 — 超快相干性的基本原理

Advances in laser technology have made it possible to produce pulses ranging from a few femtoseconds to tens of attoseconds. Learn more at Edmund Optics.

立即查看 添加到收藏夹

光束直径对激光损伤阈值的重要性

The diameter of a laser highly affects an optic’s laser induced damage (LIDT) as beam diameter directly impacts the probability of laser damage.

立即查看 添加到收藏夹

使用库存组件构建自定义光学隔离器

Edmund Optics' component list and steps provided are used to successfully build an Optical Isolator.

立即查看 添加到收藏夹

什么是分光镜?

Optical components that create two beams by splitting incident light are beamsplitters. Read more about the different types of beamsplitters at Edmund Optics.

立即查看 添加到收藏夹

了解光学参数规格

Do you want to know more about the importance of optical specifications? Learn the different types of specifications and their impact on your system at Edmund Optics.

立即查看 添加到收藏夹

激光光学实验室:激光器规格的选择

When determining which laser to use for your application, consider the following specifications: wavelength, coherence length, beam divergence, and Rayleigh range.

立即查看 添加到收藏夹

超精密抛光的光学元件

Superpolished optics with sub-angstrom surface roughness are ideal for precise laser optics applications

立即查看 添加到收藏夹

光学镀膜简介

Optical coatings are used to influence the transmission, reflection, or polarization properties of an optical component.

立即查看 添加到收藏夹

激光光学实验室:预告

The Laser Optics Lab video series discusses laser optics concepts including specifications, coating technologies, product types, and more

立即查看 添加到收藏夹

激光光学实验室:简介

The Laser Optics Lab video series discusses laser optics concepts including specifications, coating technologies, product types, and more

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号