您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 年度 Cyber 大促! (213)

4 大光学前沿

Advances in microscopy, imaging, and extreme ultraviolet optics

立即查看 添加到收藏夹

对比度

Is the definition on your image not clear? Go back to the basics and learn more about the contrast of an image and its importance at Edmund Optics.

立即查看 添加到收藏夹

75周年纪念视频

Edmund Optics helped fuel Dan Magorian's fascination with science in 1966 when he built a Edmund fiber optic tree while in middle school.

立即查看 添加到收藏夹

大视场远心镜头

Large field of view telecentric imaging lenses allow for reduction of measurement and inspection time. Learn more about large FOV lenses at Edmund Optics.

立即查看 添加到收藏夹

2014年 爱特蒙特光学公司的节日视频

As a family owned business for almost 75 years, the bond between family has long been the foundation of Edmund Optics.

立即查看 添加到收藏夹

吸收度

Light is absorbed in optical media through several methods including exciting electrons to higher energy states and converting to thermal energy

立即查看 添加到收藏夹

爱特蒙特光学70周年

Celebrate 70 years with EO! Take a journey from 1942 to 2012 and beyond.

立即查看 添加到收藏夹

远心度优点

Learn more about the advantages of telecentricity, including parallax error elimination, telecentric lenses, depth of field, and distortion, at Edmund Optics.

立即查看 添加到收藏夹

球面透镜的精度公差

Optical lenses require very precise tolerances. Learn more about tolerances for spherical lenses at Edmund Optics.

立即查看 添加到收藏夹

远心镜头大小控制

Telecentric Lenses can grow quite large and heavy with small magnifications, as such magnifications require large front optics. Learn more at Edmund Optics.

立即查看 添加到收藏夹

失真与远心度规格

Elimination of parallax and distortion play a large role in determining the quality of certain telecentric lenses. Learn more at Edmund Optics.

立即查看 添加到收藏夹

大尺寸万向节光学镜架

爱特蒙特光学(Edmund Optics)提供的大尺寸万向节光学镜架可用于将大尺寸精密光学元件(如反射镜)集成到 OEM 和台式系统中。

立即查看 添加到收藏夹

分辨率与对比度限制:艾里斑

The diffraction pattern caused when light passes through an aperture is called the Airy Disk. Find out how the Airy Disk can impact your image at Edmund Optics.

立即查看 添加到收藏夹

分辨率和对比度对比

Learn how Edmund Optics maintains optical performance across the entire image plane through this resolution and contrast comparison using our C Series FFL lens.

立即查看 添加到收藏夹

了解远场校正物镜分辨能力与放大率

Microscopes are used in a variety of fields and applications. To understand how resolving power, magnification, and other aspects work, read more at Edmund Optics.

立即查看 添加到收藏夹

金刚石车削离轴抛物反射镜的粗糙度

Learn about spatial frequency errors and surface roughness of Single Point Diamond Turned off-axis parabolic mirrors at Edmund Optics.

立即查看 添加到收藏夹

如何定义光学透镜的放大倍数

When doing basic imaging, how do you determine the magnification an optical lens will provide?

立即查看 添加到收藏夹

如何选择可变放大倍率镜头

To decide what imaging lens is right for a system, it is important to know the parameters of the imaging system used. Learn more at Edmund Optics.

立即查看 添加到收藏夹

EO成像实验室1.7:深入了解对比度

Learn how to specify imaging system components.

立即查看 添加到收藏夹

非球面透镜不规则度与斯特列尔比

The Strehl ratio of an optical system is a comparison of its real performance with its diffraction-limited performance.

立即查看 添加到收藏夹

如何选择固定放大倍率镜头

Fixed magnification lenses typically function properly at a single working distance and are specified by their magnification. Learn more at Edmund Optics.

立即查看 添加到收藏夹

光学系统机械设计、装配和校准的5大考量

Are you designing an optical system? Be sure to review these 5 considerations relating to mechanical design, assembly, and alignment at Edmund Optics.

立即查看 添加到收藏夹

认识Pat McKenna,计量大师

The Future Depends on Optics®

立即查看 添加到收藏夹

2012节日特辑:僵尸大战

Happy Holidays from EO! Friends, is this not what the holidays are all about?

立即查看 添加到收藏夹

认识Jeremy Govier,非球面大师

The Future Depends on Optics®

立即查看 添加到收藏夹

2021 年节日视频

Happy Holidays from Edmund Optics®! As we enter our 80th year of business, we would like to thank the community that has supported us over the years.

立即查看 添加到收藏夹

EO成像实验室模块2:计量和测量精度概述

Learn how to specify imaging system components.

立即查看 添加到收藏夹

认识Francis Ang,棱镜大师

The Future Depends on Optics®

立即查看 添加到收藏夹

认识Scott Sparrold,设计大师

The Future Depends on Optics®

立即查看 添加到收藏夹

Free-Space Optical Communication

Free-space optical (FSO) communications wirelessly transmit data through the air using lasers. FSO promises to revolutionize broadband internet access.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号