您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 网购节 偏振! (101)

激光器谐振模

The length of a laser resonator determines the laser’s resonator modes, or the electric field distributions that cause a standing wave in the cavity.

立即查看 添加到收藏夹

选择合适的照明

Not sure which type of illumination you should use for your system? Learn more about the pros and cons of different illumination types at Edmund Optics.

立即查看 添加到收藏夹

什么是分光镜?

Optical components that create two beams by splitting incident light are beamsplitters. Read more about the different types of beamsplitters at Edmund Optics.

立即查看 添加到收藏夹

激光光学计量

Metrology is critical for ensuring that optical components consistently meet their desired specifications, especially in laser applications.

立即查看 添加到收藏夹

何谓成像?

在成像过程中,光线通过成像镜头从物体映射到成像传感器上,以再现物体的特征和相似性,从而达到检查、分类或分析的目的。

立即查看 添加到收藏夹

光学系统机械设计、装配和校准的5大考量

Are you designing an optical system? Be sure to review these 5 considerations relating to mechanical design, assembly, and alignment at Edmund Optics.

立即查看 添加到收藏夹

激光系统的关键参数

了解确保激光应用成功必须考虑的关键参数。将为这些参数建立通用术语。

立即查看 添加到收藏夹

成像镜头的加固

Have an application in a demanding environment? Learn about the different types of ruggedization: industrial, ingress protection, and stability at Edmund Optics.

立即查看 添加到收藏夹

高激光损伤AR镀膜

Laser optics high reflectivity mirrors meet exceptional specifications that Edmund Optics' competitors often fail to meet. Learn more at Edmund Optics.

立即查看 添加到收藏夹

使用库存组件构建自定义光学隔离器

Edmund Optics' component list and steps provided are used to successfully build an Optical Isolator.

立即查看 添加到收藏夹

光学镀膜简介

Optical coatings are used to influence the transmission, reflection, or polarization properties of an optical component.

立即查看 添加到收藏夹

散射

Dispersion is the dependence of the phase velocity or phase delay of light on another parameter, such as wavelength, propagation mode, or polarization.

立即查看 添加到收藏夹

5 个技巧适用于利用现货光学件进行设计

Have a time or budget restraint? Check out these tips and advantages for designing applications with standard, off-the-shelf optics at Edmund Optics.

立即查看 添加到收藏夹

夹杂物和气泡的均匀性和散射

Inhomogeneity and scatter from inclusions and bubbles in optical components can lead to worse performance, especially in laser optics applications.

立即查看 添加到收藏夹

液态镜头介绍

Imaging lens performance can be enhanced with the use of liquid lenses. Learn more at Edmund Optics.

立即查看 添加到收藏夹

使用结构化照明

Machine vision systems heavily rely on illumination. Learn more about how structured illumination can maximize your system at Edmund Optics.

立即查看 添加到收藏夹

了解显微镜和物镜

Learn about the different components used to build a microscope, key concepts, and specifications at Edmund Optics.

立即查看 添加到收藏夹

成像电子元件101:基本数字相机设置知识,改善您的成像效果

Do you want to improve your imaging results? Go back to the basics of camera settings, learn how these important aspects can affect your image at Edmund Optics.

立即查看 添加到收藏夹

成像基本参数

想要了解成像的基本概念?在 Edmund Optics 了解更多有关基本术语及成像行业应用的相关信息。

立即查看 添加到收藏夹

高功率光学镀膜的复杂情况

Want to know more about high-power optical coatings? Find out more about the importance, fabrication, and testing at Edmund Optics.

立即查看 添加到收藏夹

远心度优点

Learn more about the advantages of telecentricity, including parallax error elimination, telecentric lenses, depth of field, and distortion, at Edmund Optics.

立即查看 添加到收藏夹

形状因素对非球面设计的影响

Learn how the shape factor of an aspheric lens effects its performance and when certain shape factors are the most advantageous.

立即查看 添加到收藏夹

光学棱镜简介

Learn about the different types of optical prisms, their applications, and how to select the right prism for your specific system.

立即查看 添加到收藏夹

球面透镜的精度公差

Optical lenses require very precise tolerances. Learn more about tolerances for spherical lenses at Edmund Optics.

立即查看 添加到收藏夹

分辨率

Do you want to understand how a lens works? To do so, you must learn key terms for how the lens functions, including resolution. Find out more at Edmund Optics.

立即查看 添加到收藏夹

了解并指定激光元件的激光损伤阈值(LIDT)

Laser induced damage threshold (LIDT) denotes the maximum laser fluence an optical component can withstand with an acceptable amount of risk.

立即查看 添加到收藏夹

使用柱面透镜时的其他考虑事项

Learn about specifications that should be considered when using cylinder lenses, including power axis wedge, plano axis wedge, and axial twist at Edmund Optics.

立即查看 添加到收藏夹

高反射率镀膜

Highly reflective (HR) coatings are applied to optical components to minimize losses when reflecting lasers and other light sources.

立即查看 添加到收藏夹

超快激光的激光损伤阈值

The short pulse durations of ultrafast lasers make them interact with optical components differently, impacting the optic’s laser damage threshold.

立即查看 添加到收藏夹

了解光学参数规格

Do you want to know more about the importance of optical specifications? Learn the different types of specifications and their impact on your system at Edmund Optics.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号