您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 年度 Cyber 大促! (116)

对比度

Is the definition on your image not clear? Go back to the basics and learn more about the contrast of an image and its importance at Edmund Optics.

立即查看 添加到收藏夹

吸收度

Light is absorbed in optical media through several methods including exciting electrons to higher energy states and converting to thermal energy

立即查看 添加到收藏夹

远心度优点

Learn more about the advantages of telecentricity, including parallax error elimination, telecentric lenses, depth of field, and distortion, at Edmund Optics.

立即查看 添加到收藏夹

球面透镜的精度公差

Optical lenses require very precise tolerances. Learn more about tolerances for spherical lenses at Edmund Optics.

立即查看 添加到收藏夹

远心镜头大小控制

Telecentric Lenses can grow quite large and heavy with small magnifications, as such magnifications require large front optics. Learn more at Edmund Optics.

立即查看 添加到收藏夹

失真与远心度规格

Elimination of parallax and distortion play a large role in determining the quality of certain telecentric lenses. Learn more at Edmund Optics.

立即查看 添加到收藏夹

分辨率与对比度限制:艾里斑

The diffraction pattern caused when light passes through an aperture is called the Airy Disk. Find out how the Airy Disk can impact your image at Edmund Optics.

立即查看 添加到收藏夹

分辨率和对比度对比

Learn how Edmund Optics maintains optical performance across the entire image plane through this resolution and contrast comparison using our C Series FFL lens.

立即查看 添加到收藏夹

了解远场校正物镜分辨能力与放大率

Microscopes are used in a variety of fields and applications. To understand how resolving power, magnification, and other aspects work, read more at Edmund Optics.

立即查看 添加到收藏夹

金刚石车削离轴抛物反射镜的粗糙度

Learn about spatial frequency errors and surface roughness of Single Point Diamond Turned off-axis parabolic mirrors at Edmund Optics.

立即查看 添加到收藏夹

如何选择可变放大倍率镜头

To decide what imaging lens is right for a system, it is important to know the parameters of the imaging system used. Learn more at Edmund Optics.

立即查看 添加到收藏夹

非球面透镜不规则度与斯特列尔比

The Strehl ratio of an optical system is a comparison of its real performance with its diffraction-limited performance.

立即查看 添加到收藏夹

如何选择固定放大倍率镜头

Fixed magnification lenses typically function properly at a single working distance and are specified by their magnification. Learn more at Edmund Optics.

立即查看 添加到收藏夹

光学系统机械设计、装配和校准的5大考量

Are you designing an optical system? Be sure to review these 5 considerations relating to mechanical design, assembly, and alignment at Edmund Optics.

立即查看 添加到收藏夹

何谓成像?

在成像过程中,光线通过成像镜头从物体映射到成像传感器上,以再现物体的特征和相似性,从而达到检查、分类或分析的目的。

立即查看 添加到收藏夹

成像电子元件101:了解适用于机器视觉应用的相机传感器

The performance of an imaging system relies on a number of things, including imaging electronics. Before using your imaging system, learn about camera sensors at Edmund Optics.

立即查看 添加到收藏夹

硬镀膜的益处

Hard coatings provide many advantages compared to traditional soft coated optics. Learn more about the coating differences and benefits at Edmund Optics.

立即查看 添加到收藏夹

高斯光束传播

Understanding Gaussian beam propagation is critical for understanding laser systems because many lasers are assumed to have Gaussian profiles.

立即查看 添加到收藏夹

从镜头到传感器: 信息采集限制

Trying to understand how much information you can obtain from a lens and sensor? Learn more about the limitations of collecting data at Edmund Optics.

立即查看 添加到收藏夹

超快激光的激光损伤阈值

The short pulse durations of ultrafast lasers make them interact with optical components differently, impacting the optic’s laser damage threshold.

立即查看 添加到收藏夹

光学玻璃

Choosing the right optical glass is important. Find out factors and properties on how to select the right optical glass at Edmund Optics.

立即查看 添加到收藏夹

成像电子元件101:适用于机器视觉应用的相机类型和接口

Are you new to imaging or looking for a refresh on camera types? Learn about the advantages to camera types, digital interfaces, and more at Edmund Optics.

立即查看 添加到收藏夹

平行的考虑事项

Optical considerations for collimating various types real and ideal point sources. Learn more at Edmund Optics.

立即查看 添加到收藏夹

了解稀土材料

Rare earth materials are used in many optics. Find an explanation, examples, and more information about rare earths at Edmund Optics.

立即查看 添加到收藏夹

所有关于非球面透镜

Learn all about the benefits of aspheres, their unique anatomy, how they're manufactured, and how to choose the right one for your system.

立即查看 添加到收藏夹

了解白色扩散玻璃

Learn more about White Diffusing Glass, which reduces the scattering of light and homogenizes the light source, at Edmund Optics.

立即查看 添加到收藏夹

什么是超薄滤光片?

How are ultra-thin filters different from standard optical filters? Discover the unique features and capabilties of ultra-thin filters at Edmund Optics.

立即查看 添加到收藏夹

光学基片的热力学性质

The thermal properties of optical substrates including the CTE, dn/dT, and thermal conductivity are critical for predicting real-world performance

立即查看 添加到收藏夹

根据分辨率选择镜头

The modulation transfer function of a lens varies depending on working distance, sensor size, f/#, and wavelength. Learn more at Edmund Optics.

立即查看 添加到收藏夹

分辨率

Do you want to understand how a lens works? To do so, you must learn key terms for how the lens functions, including resolution. Find out more at Edmund Optics.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号