您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: 中性密度(ND)滤光片 (122)

光学滤光片

Do you want to learn about optical filters? Find terminology, fabrication techniques, a selection guide, and application examples at Edmund Optics.

立即查看 添加到收藏夹

什么是超薄滤光片?

How are ultra-thin filters different from standard optical filters? Discover the unique features and capabilties of ultra-thin filters at Edmund Optics.

立即查看 添加到收藏夹

荧光团和光学滤光片以进行荧光显微

Want to know more about fluorophores and optical filters for fluorescence microscopy? Find out more information and in stock optical filters at Edmund Optics.

立即查看 添加到收藏夹

荧光显微镜:内置了照明和滤光片用于成像

Want to know about fluorescence microscopy? Read this article by a Biomedical Product Line Engineer at Edmund Optics to learn more.

立即查看 添加到收藏夹

光学基片的热力学性质

The thermal properties of optical substrates including the CTE, dn/dT, and thermal conductivity are critical for predicting real-world performance

立即查看 添加到收藏夹

LIDT 规范中的 不确定性

Laser induced damage threshold (LIDT) of optics is a statistical value influenced by defect density, the testing method, and fluctuations in the laser.

立即查看 添加到收藏夹

了解精密定位中的误差源

Understanding the source of inaccurate and imprecise errors can help formulate strategies to prevent or correct them. Learn more at Edmund Optics.

立即查看 添加到收藏夹

光束直径对激光损伤阈值的重要性

The diameter of a laser highly affects an optic’s laser induced damage (LIDT) as beam diameter directly impacts the probability of laser damage.

立即查看 添加到收藏夹

超快激光 — 超快相干性的基本原理

Advances in laser technology have made it possible to produce pulses ranging from a few femtoseconds to tens of attoseconds. Learn more at Edmund Optics.

立即查看 添加到收藏夹

吸收度

Light is absorbed in optical media through several methods including exciting electrons to higher energy states and converting to thermal energy

立即查看 添加到收藏夹

了解波片和延迟器

Waveplates (retarders) are different when used in polarized light than unpolarized light. Consider terminology, fabrication, or applications at Edmund Optics.

立即查看 添加到收藏夹

球面透镜的精度公差

Optical lenses require very precise tolerances. Learn more about tolerances for spherical lenses at Edmund Optics.

立即查看 添加到收藏夹

了解光学参数规格

Do you want to know more about the importance of optical specifications? Learn the different types of specifications and their impact on your system at Edmund Optics.

立即查看 添加到收藏夹

带有激光照明的荧光成像

Fluorescence imaging systems are composed of three major components, an illumination source, a photo-activated fluorophore sample, and detector.

立即查看 添加到收藏夹

高激光损伤AR镀膜

Laser optics high reflectivity mirrors meet exceptional specifications that Edmund Optics' competitors often fail to meet. Learn more at Edmund Optics.

立即查看 添加到收藏夹

激光扩束镜

Laser beam expanders are critical for reducing power density, minimizing beam diameter at a distance, and minimizing focused laser spot size.

立即查看 添加到收藏夹

夹杂物和气泡的均匀性和散射

Inhomogeneity and scatter from inclusions and bubbles in optical components can lead to worse performance, especially in laser optics applications.

立即查看 添加到收藏夹

高功率光学镀膜的复杂情况

Want to know more about high-power optical coatings? Find out more about the importance, fabrication, and testing at Edmund Optics.

立即查看 添加到收藏夹

镜头性能曲线

Are you trying to measure the performance of your lens? Although this can be a difficult task, there are curves that can help. Read more at Edmund Optics.

立即查看 添加到收藏夹

传感器的相对照明、衰减与光晕

In order to understand vignetting, it is important to understand sensor sizes, formats, and roll-off and relative illumination. Find out more at Edmund Optics.

立即查看 添加到收藏夹

激光损伤阈值测试

Testing laser induced damage threshold (LIDT) is not standardized, so understanding how your optics were tested is critical for predicting performance.

立即查看 添加到收藏夹

对比度

Is the definition on your image not clear? Go back to the basics and learn more about the contrast of an image and its importance at Edmund Optics.

立即查看 添加到收藏夹

远心照明:为何机器视觉应用中需要它

Think you don't need telecentric illumination in machine vision applications? Find out why you need telecentric illumination at Edmund Optics.

立即查看 添加到收藏夹

了解并指定激光元件的激光损伤阈值(LIDT)

Laser induced damage threshold (LIDT) denotes the maximum laser fluence an optical component can withstand with an acceptable amount of risk.

立即查看 添加到收藏夹

光学笼式系统设计示例

Not sure how you can enhance an opical cage system? Check out examples of different design examples applicable for small and large systems at Edmund Optics.

立即查看 添加到收藏夹

在红外应用中使用弯月透镜的优势

Meniscus lenses offer superior performance compared to plano convex lenses in IR applications. Find out the benefits of using a meniscus lens at Edmund Optics.

立即查看 添加到收藏夹

金刚石车削离轴抛物反射镜的粗糙度

Learn about spatial frequency errors and surface roughness of Single Point Diamond Turned off-axis parabolic mirrors at Edmund Optics.

立即查看 添加到收藏夹

波长对性能的影响

Wavelengths can be both valuable or hazardous when trying to obtain information from an imaging system. Learn more about fixing wavelength issues at Edmund Optics.

立即查看 添加到收藏夹

激光系统的关键参数

了解确保激光应用成功必须考虑的关键参数。将为这些参数建立通用术语。

立即查看 添加到收藏夹

光学镀膜简介

Optical coatings are used to influence the transmission, reflection, or polarization properties of an optical component.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号